Missing i.MX8 DDR Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing i.MX8 DDR Tool

Jump to solution
1,247 Views
allenivester
Contributor III

I am trying to run the i.MX8 DDR Tool for a new i.MX8M mini board, as referenced in this post:

https://community.nxp.com/docs/DOC-340179 

But there's no tool there.  The post (and others) refer to a GUI tool and user guide in the "package", but the only zip file in the attachments just contains a bunch of SPL binaries, none of which are for i.MX8.  I did manage to find a GUI "NXP DDR Test Tool" from another MX6/7-specific post, but the TARGET field in the GUI also does not have any i.MX8 choices, and the u-boot binaries included with that package are only for mx6/7.  And there's no user guide.

I see that the i.MX8 MSCALE SERIES DDR Tool Release (V3.00) post was updated only a few hours ago.  Is it possible that the zip file containing the actual tool was accidentally removed?  I wish I could see the history of that post, like you can with most wikis.

Labels (1)
0 Kudos
1 Solution
1,074 Views
oliver_chen
NXP Employee
NXP Employee

Hi Allen,

I'm sorry for that. I've uploaded the correct packages and you can download now.

B.R

Oliver

View solution in original post

0 Kudos
2 Replies
1,075 Views
oliver_chen
NXP Employee
NXP Employee

Hi Allen,

I'm sorry for that. I've uploaded the correct packages and you can download now.

B.R

Oliver

0 Kudos
1,074 Views
allenivester
Contributor III

Excellent!  Thank you.  The stress test works fine with my .ds file.

0 Kudos