Hello ;
I have been working on writing mipi csi-2 imx290 camera driver. I have faced with csi_mclk error.
This is imx290 probe function ;
static int imx290_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
struct device *dev = &client->dev;
int retval;
int value;
/* request reset pin */
xclr = of_get_named_gpio(dev->of_node, "rst-gpios", 0);
if (!gpio_is_valid(xclr)) {
dev_warn(dev, "no sensor reset pin available");
return -EINVAL;
}
retval = devm_gpio_request_one(dev, xclr, GPIOF_OUT_INIT_LOW,"imx290_mipi_reset");
if (retval < 0)
return retval;
/* Set initial values for the sensor struct. */
memset(&imx290_data, 0, sizeof(imx290_data));
imx290_data.sensor_clk = devm_clk_get(dev, "csi_mclk");
if (IS_ERR(imx290_data.sensor_clk)) {
/* assuming clock enabled by default */
imx290_data.sensor_clk = NULL;
dev_err(dev, "clock-frequency missing or invalid\n");
return PTR_ERR(imx290_data.sensor_clk);
}
retval = of_property_read_u32(dev->of_node, "mclk",&(imx290_data.mclk));
if (retval) {
dev_err(dev, "mclk missing or invalid\n");
return retval;
}
retval = of_property_read_u32(dev->of_node, "mclk_source",
(u32 *) &(imx290_data.mclk_source));
if (retval) {
dev_err(dev, "mclk_source missing or invalid\n");
return retval;
}
retval = of_property_read_u32(dev->of_node, "csi_id",
&(imx290_data.csi));
if (retval) {
dev_err(dev, "csi id missing or invalid\n");
return retval;
}
clk_prepare_enable(imx290_data.sensor_clk);
imx290_data.io_init = imx290_reset;
imx290_data.i2c_client = client;
imx290_data.pix.pixelformat = V4L2_PIX_FMT_UYVY;
imx290_data.pix.width = 1920;
imx290_data.pix.height = 1080;
imx290_data.streamcap.capability = V4L2_MODE_HIGHQUALITY | V4L2_CAP_TIMEPERFRAME;
imx290_data.streamcap.capturemode = 0;
imx290_data.streamcap.timeperframe.denominator = DEFAULT_FPS;
imx290_data.streamcap.timeperframe.numerator = 1;
imx290_power_on(dev);
imx290_reset();
retval = imx290_write_reg(IMX290_REG_STANDBY, 0x1,NULL);
imx290_int_device.priv = &imx290_data;
retval = v4l2_int_device_register(&imx290_int_device);
clk_disable_unprepare(imx290_data.sensor_clk);
pr_info("camera imx290_mipi is found\n");
return retval;
}
This is the device tree;
imx290_mipi: imx290_mipi@1a {
compatible = "sony,imx290lqr,imx290,imx290_camera";
reg = <0x1a>;
clocks = <&clks 200>;
clock-names = "csi_mclk";
OVDD = <®_1p8v>;
AVDD = <®_2p9v>;
DVDD = <®_1p2v>;
pwn-gpios = <&gpio1 6 1>;
rst-gpios = <&gpio4 14 0>; /// xclr
ipu_id = <0>;
csi_id = <0>;
mclk = <37125000>;
mclk_source = <0>;
lanes = <4>;
I think the csi_mclk should be taken from device tree without any error because it is just a device driver macro and imx290_data.sensor_clk = devm_clk_get(dev, "csi_mclk"); should work but I dont understand what is wrong ? My mind confused a lot while trying to solve this problem , I need help about that.
Thanks
Best Regards
Hi Mustafa
please check with oscilloscope mclk on clko2:
https://community.nxp.com/thread/309260
and check its initialization in clk-imx6q.c:
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/mach-imx/clk-imx6q.c?h=imx_4.1...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------