Hi chip experts,
I found 2 descriptions about vpu_IsBusy() in i.MX5x_Linux_VPU_API.pdf.
  (1) Figure 4. Decoder Operation Flow on p41 
  (2) 4.3.3.5 Completion of Picture Decoding on p86
Is it possible to replace vpu_IsBusy() call with vpu_WaitForInt()?
Because I prefer interrupt rather than polling.
If yes, are any modifications need except above swap?
Can anyone help me?
Thanks.
Hi torus1000
yes it can be used, example can be found in imx-test package
(one needs to select it in ltib)
imx-test-11.09.01/test/mxc_vpu_test/dec.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Thank you for reply.
I confirmed dec.c code included 2 of vpu_WaitForInt(). I'm not sure both of them looks the same as msleep(500).
( 1st one use for vpu reset when hung around 10x500ms. 2nd one rarely use only when vpu_IsBusy==false.)
Regard to dec.c (see below),
Is it possible to replace vpu_IsBusy() with vpu_WaitForInt()?
BR
is_waited_int = 0;
//line896
while (vpu_IsBusy()) {
err = dec_fill_bsbuffer(handle, dec->cmdl,
...
/* * Suppose vpu is hang if one frame cannot be decoded in 5s,
* then do vpu software reset. */
//line917
if (!err) {
vpu_WaitForInt(500);
is_waited_int = 1;
loop_id ++;
}
}
//line925
if (!is_waited_int)
vpu_WaitForInt(500);
Hi torus1000
yes, I think it is possible to replace vpu_IsBusy() with vpu_WaitForInt()
Best regards
igor
Dear Igor,
We customized wait flow as following;
vpu_DecStartOneFrame();
for(i=0;i<30;i++){
if(SUCCESS == vpu_WaitForInt(Wait time)) break;
vpu_DecGetBitstreamBuffer();
vpu_DecUpdateBitstreamBuffer();
}
if(i<30) vpu_DecGetOutputInfo();
else <Abnormal termination processing>
It worked for now.
(Q) Do you think our flow have no problems?
If somethig wrong, please let us know. Thank you for your kndly reply.
Best Regards.
Hi torus1000
sorry for delay.
I think these codes have not problems.
Best regards
igor
Dear Igor,
I really appreciate to your reply.
If you also have some hints about my previous questions, please let me know. (I have to make a report.)
> Why did vpu_IsBusy sometimes continue to return 1 around 25 sec?
Thanks.
Hi torus1000
vpu_IsBusy may return even no vpu interrupt produced, just after timeout.
According to its description:
The application waits for the decoder or encoder to completed the interrupt. This function returns
immediately if the interrupt has been received, otherwise, it returns after timeout_in_ms.
Best regards
igor
Dear Igor,
Actually We replaced vpu_IsBusy() with vpu_WaitForInt() but vpu sometimes stopped decoding.
Then we tried both as following order just in case; vpu_WaitForInt -> vpu_IsBusy
The result looks OK in most case. But sometimes vpu state kept in busy in spite of Operation successfully completed.
(OK) vpu_WaitForInt -> vpu_IsBusy
return RETCODE_SUCCESS return 0(FAIL) vpu_WaitForInt -> vpu_IsBusy -> after 25 sec, vpu_IsBusy
return RETCODE_SUCCESS return 1 return 0
"Operation successful" "busy" "idle"
Why did vpu_IsBusy sometimes continue to return 1 around 25 sec?
If you know something about this, please let us know because we need the reason to make sort of failure analysis report.
Thanks.