Minimum interval i.MX6 read -> write and write -> read cycle.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum interval i.MX6 read -> write and write -> read cycle.

Jump to solution
1,147 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 some interface.

Please see the attached file.

If user repeat read -> write -> read -> write -> ... on the following interfaces, could you let me know the minimum interval between read -> write and write -> read?

GPMI (NAND Fhash)

USB

uSDHC (SD card)

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
931 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid it is not possible to answer on that since

internal delays are impossible to predict or calculate.

For example with 8-8-8 DDR and tRALAT =5 one can have

about 50ns @532 MHz just for accessing data from memory.

Latencies caused by OS can be found below

LMbench Benchmarks on i.MX.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
932 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid it is not possible to answer on that since

internal delays are impossible to predict or calculate.

For example with 8-8-8 DDR and tRALAT =5 one can have

about 50ns @532 MHz just for accessing data from memory.

Latencies caused by OS can be found below

LMbench Benchmarks on i.MX.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply