Minimal resolution on LVDS, iMX6S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimal resolution on LVDS, iMX6S

Jump to solution
2,144 Views
cerma
Contributor IV

Hello, what is minimal resolution on LVDS? I saw in datasheet that minimal frequency is 0 - 85 MHz but there was also mentioned that minimal frequency is 25 MHz. I need to set 480x272 (frequency about 9 MHz) but I don't know if is that even possible. Is it possible to set this resolution, if so, how?

0 Kudos
Reply
1 Solution
1,509 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

View solution in original post

0 Kudos
Reply
2 Replies
1,510 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

0 Kudos
Reply
1,509 Views
haitao
Contributor II

你好,weidong!

按照你的方法,我得到的时钟最低为25.6M,我得不到9M的时钟。不知道为什么

0 Kudos
Reply