Hello,
I have an imx7s warp7 that is not renumerating midway through updating the board's image using mfgtool.
When mfgtool loads a new image it loads up uboot, initramsfs and UTP creating a mass-storage gadget, after which it should renumerate and continue loading the real image, fs etc.
The problem I'm experiencing is that the warp7 hangs once the UTP mass-storage device has been created. The only way to proceed with loading the second half of mfgtools's transfer is to quickly pull out the usb lead and reinsert. This causes windows to detect the new mass-storage device and mfgtool carries on to complete is overall job. In production this need to be automatic as it should be.
Any advice would be appreciated.