Mfgtool download ERR for MCIMX6Q-SDB board(REV B5)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mfgtool download ERR for MCIMX6Q-SDB board(REV B5)

1,012 Views
soursunny
Contributor II

Hi all,

     I'm working on the MCIMX6Q-SDB board(REV B5). When i use the mfgtool(Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER) to download Android 4.2.2 prebuilt image , it return err.

U-Boot 2009.08 (Jun 02 2013 - 23:06:16)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 189

Temperature:   47 C, calibration data 0x5ae4e87d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-SABRESD: RevC Board: 0x63312 [POR ]

Boot Device: SPI NOR

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Using default environment

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:04:9f:02:66:c3

FEC0 [PRIME]

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2563-gd970361

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3162980 Bytes =  3 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 10c00000 ...

   Image Name:   uboot initramfs rootfs

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    4543831 Bytes =  4.3 MB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Linux version 3.0.35-2563-gd970361 (b43083@bluemeany) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Sun Jun 2 22:56:58 CDT 2013

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @8c008000 s5184 r8192 d15296 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc enable_wait_mode=off

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1024MB = 1024MB total

Memory: 1028692k/1028692k available, 19884k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

    vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x8003a000   ( 200 kB)

      .text : 0x8003a000 - 0x805ada2c   (5583 kB)

      .data : 0x805ae000 - 0x805fc800   ( 314 kB)

       .bss : 0x805fc824 - 0x80627774   ( 172 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

No AHCI save PWR: PDDQ enabled

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

bio: create slab <bio-0> at 0

mxs-dma mxs-dma-apbh: initialized

print_constraints: SPKVDD: 4200 mV

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 0

mc_pfuze 1-0008: FAB: 0 ,FIN: 0

PF100 1.0 chip found!

print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV

print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV

print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 3000 mV

print_constraints: PFUZE100_VREFDDR: at 750 mV

print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2500 mV

print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2800 mV

print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

max17135 2-0048: PMIC MAX17135 for eInk display

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

Clockevents: could not switch to one-shot mode:

Clockevents: could not switch to one-shot mode:

Clockevents: could not switch to one-shot mode:

Clockevents: could not switch to one-shot mode: dummy_timer is not functional.

dummy_timer is not functional.

dummy_timer is not functional.

Could not switch to high resolution mode on CPU 0

Could not switch to high resolution mode on CPU 1

Could not switch to high resolution mode on CPU 3

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Unpacking initramfs...

dummy_timer is not functional.

Could not switch to high resolution mode on CPU 2

Freeing initrd memory: 4436K

PMU: registered new PMU device of type 0

Static Power Management for Freescale i.MX6

wait mode is disabled for i.MX6

cpaddr = c0880000 suspend_iram_base=c091c000

PM driver module loaded

IMX usb wakeup probe

cpu regulator mode:ldo_bypass

_regulator_get: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

Internal error: Oops - undefined instruction: 0 [#1] PREEMPT SMP

Modules linked in:

CPU: 2    Not tainted  (3.0.35-2563-gd970361 #1)

PC is at put_filp+0x10/0x7c

LR is at path_openat+0xf0/0x3a4

pc : [<800ec6c8>]    lr : [<800f7c00>]    psr: 60000013

sp : bda47e90  ip : 00000000  fp : 000a491c

r10: 00000000  r9 : bda46000  r8 : bda46000

r7 : bda47eb4  r6 : fffffffe  r5 : bda47f78  r4 : bfeb6460

r3 : bfeb6480  r2 : 00000000  r1 : 00000000  r0 : bfeb6460

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4da7c04a  DAC: 00000015

Process hotplug (pid: 478, stack limit = 0xbda462f0)

Stack: (0xbda47e90 to 0xbda48000)

7e80:                                     bda47f78 fffffffe bda47ef8 800f7c00

7ea0: bda47ec4 000003ff 00000000 bda47f80 bda46000 bffc30a0 be027bb0 800ea8cc

7ec0: 000003ff 00000000 805fbb40 00000003 bda47f78 bd931000 ffffff9c ffffff9c

7ee0: bda46000 00000000 000a491c 800f7f90 00000043 2ac55d34 bffc30a0 be027bb0

7f00: ab3df08e 0000000c bd93100f bffc30a0 be002088 be082000 00000103 00000004

7f20: 00000000 00000000 bfd16570 000a7e00 805c3d14 000a7dec bff197e0 bff197e8

7f40: 00000000 bff19820 000a4800 000a4801 00000000 bfeb6460 000a7dec bd931000

7f60: 000a4800 00000000 00000003 800ea444 7ed2e7ec 00000000 000a4800 00000000

7f80: 00000024 00000100 00200200 000a7e1c 000a7e00 000a7dec 00000005 800400c4

7fa0: 00000000 8003ff40 000a7e1c 000a7e00 000a7e00 000a4800 000a7dec 0000002f

7fc0: 000a7e1c 000a7e00 000a7dec 00000005 7ed2e840 000a6a5c 000a7e00 000a491c

7fe0: 2ac55d34 7ed2e75c 00038048 2ac55d54 20000010 000a7e00 67a11877 438313c7

[<800ec6c8>] (put_filp+0x10/0x7c) from [<800f7c00>] (path_openat+0xf0/0x3a4)

[<800f7c00>] (path_openat+0xf0/0x3a4) from [<800f7f90>] (do_filp_open+0x2c/0x80)

[<800f7f90>] (do_filp_open+0x2c/0x80) from [<800ea444>] (do_sys_open+0xdc/0x174)

[<800ea444>] (do_sys_open+0xdc/0x174) from [<8003ff40>] (ret_fast_syscall+0x0/0x30)

Code: e92d4010 e2803020 e24dd008 e1a04000 (f77ff05f)

Internal error: Oops - undefined instruction: 0 [#2] PREEMPT SMP

---[ end trace 86a7da615f57aaeb ]---

Modules linked in:

CPU: 0    Tainted: G      D      (3.0.35-2563-gd970361 #1)

PC is at put_filp+0x10/0x7c

LR is at path_openat+0xf0/0x3a4

pc : [<800ec6c8>]    lr : [<800f7c00>]    psr: 60000013

sp : bdabde90  ip : 00000000  fp : 00000000

r10: 00000000  r9 : bdabc000  r8 : bdabc000

r7 : bdabdeb4  r6 : fffffffe  r5 : bdabdf78  r4 : bda5f140

r3 : bda5f160  r2 : 00000000  r1 : 00000000  r0 : bda5f140

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4dac004a  DAC: 00000015

Process hotplug (pid: 484, stack limit = 0xbdabc2f0)

Stack: (0xbdabde90 to 0xbdabe000)

de80:                                     bdabdf78 fffffffe bdabdef8 800f7c00

dea0: bdabdec4 bdabdf08 bffc30a0 be0a3a18 00001000 bffc30a0 be0a3908 00000000

dec0: 00000001 00000000 bdabdf00 00000001 bdabdf78 bffed000 ffffff9c ffffff9c

dee0: bdabc000 00000000 00000000 800f7f90 00000041 2ab0426c bffc30a0 be0a3908

df00: e2a6dd9b 0000000b bffed005 bffc30a0 be002088 be07a2e0 00000101 00000004

df20: 00000000 00000000 00000000 2ab15adc 805c3d14 00000001 bff19a80 bff19a88

df40: 00000000 bff19ac0 00000000 00000001 00000000 bda5f140 00000001 bffed000

df60: 00000000 00000000 00000001 800ea444 2ab15358 800f7f5c 00000000 00000000

df80: 00000024 00000100 000102f0 2ab208b4 2ab208b8 00000001 00000005 800400c4

dfa0: 00000000 8003ff40 2ab208b4 2ab208b8 2ab15adc 00000000 00000001 00000000

dfc0: 2ab208b4 2ab208b8 00000001 00000005 00000000 0000a149 00000001 00000000

dfe0: 2ab20b40 7ea41510 2ab0a7e4 2ab10f5c 60000010 2ab15adc cfffdc3d ffffcf51

[<800ec6c8>] (put_filp+0x10/0x7c) from [<800f7c00>] (path_openat+0xf0/0x3a4)

[<800f7c00>] (path_openat+0xf0/0x3a4) from [<800f7f90>] (do_filp_open+0x2c/0x80)

[<800f7f90>] (do_filp_open+0x2c/0x80) from [<800ea444>] (do_sys_open+0xdc/0x174)

[<800ea444>] (do_sys_open+0xdc/0x174) from [<8003ff40>] (ret_fast_syscall+0x0/0x30)

Code: e92d4010 e2803020 e24dd008 e1a04000 (f77ff05f)

---[ end trace 86a7da615f57aaec ]---

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

msgmni has been set to 2017

cryptodev: driver loaded.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Unable to handle kernel paging request at virtual address 10446000

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

pgd = bc07c000

[10446000] *pgd=00000000

Internal error: Oops: 5 [#3] PREEMPT SMP

Modules linked in:

CPU: 3    Tainted: G      D      (3.0.35-2563-gd970361 #1)

PC is at kmem_cache_alloc+0xd4/0x110

LR is at anon_vma_fork+0x58/0x134

pc : [<800e7678>]    lr : [<800dbb4c>]    psr: 60000093

sp : bc16fe90  ip : 00000001  fp : 00001473

r10: 805c3cc0  r9 : 10446000  r8 : 00000000

r7 : 0bfe8000  r6 : 10446000  r5 : 000000d0  r4 : bfff2200

r3 : bc16e000  r2 : 805c3cc0  r1 : 8003c100  r0 : 20000013

Flags: nZCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4c07c04a  DAC: 00000015

Process hotplug (pid: 659, stack limit = 0xbc16e2f0)

Stack: (0xbc16fe90 to 0xbc170000)

fe80:                                     bffe1d98 800dbb4c bfee27b0 bfee2d20

fea0: bc14c5d8 bc14c268 80608d60 00000000 00000003 bc14c910 be07167c 800dbb4c

fec0: bc14c5d8 bfe73ba0 bc14c268 bc16e000 bc14c90c 800713b0 bdaa3b68 00000020

fee0: 00000020 bc14c8fc bc14c8f0 bfe73860 bfe7389c bfe73bdc be0020d4 bfcceb80

ff00: 01200011 bc16e000 bc093b80 805fdd40 bfcceca4 00000000 00000000 80071eac

ff20: 00000246 00000000 00000000 bfcced1c 7e955248 bc16ffb0 000000c3 00000000

ff40: bc16e000 01200011 00000000 bc16ffb0 00000000 7e955248 bc16e000 00000000

ff60: 7e955274 80072484 2aaf7068 00000000 00000000 00000000 00000001 2de54484

ff80: 51ac142f 00000000 00000001 02625a04 2aaf7068 7e955248 2acf1000 00000078

ffa0: 800400c4 8003ff40 00000000 2aaf7068 01200011 00000000 00000000 00000000

ffc0: 2aaf7068 7e955248 2acf1000 00000078 00000293 00000000 000a73ac 7e955274

ffe0: 2aaf74c0 7e955248 00000000 2ac61b48 60000010 01200011 5c56af62 a9fd7000

[<800e7678>] (kmem_cache_alloc+0xd4/0x110) from [<800dbb4c>] (anon_vma_fork+0x58/0x134)

[<800dbb4c>] (anon_vma_fork+0x58/0x134) from [<800713b0>] (dup_mm+0x184/0x46c)

[<800713b0>] (dup_mm+0x184/0x46c) from [<80071eac>] (copy_process+0x7cc/0xce4)

[<80071eac>] (copy_process+0x7cc/0xce4) from [<80072484>] (do_fork+0x9c/0x264)

[<80072484>] (do_fork+0x9c/0x264) from [<8003ff40>] (ret_fast_syscall+0x0/0x30)

Code: 1affffe9 e5948014 e28bb004 e3a0c001 (e7968008)

---[ end trace 86a7da615f57aaed ]---

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Unable to handle kernel paging request at virtual address 10446000

pgd = 80004000

[10446000] *pgd=00000000

Internal error: Oops: 5 [#4] PREEMPT SMP

Modules linked in:

CPU: 3    Tainted: G      D      (3.0.35-2563-gd970361 #1)

PC is at kmem_cache_alloc+0xd4/0x110

LR is at anon_vma_prepare+0x2c/0x168

pc : [<800e7678>]    lr : [<800db6ac>]    psr: 60000193

sp : bc027d90  ip : 00000001  fp : 00001473

r10: 805c3cc0  r9 : 10446000  r8 : 00000000

r7 : 0bfe8000  r6 : 10446000  r5 : 000000d0  r4 : bfff2200

r3 : bc026000  r2 : 805c3cc0  r1 : 8003c100  r0 : 20000113

Flags: nZCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 4c07c04a  DAC: 00000015

Process kworker/u:0 (pid: 668, stack limit = 0xbc0262f0)

Stack: (0xbc027d90 to 0xbc028000)

7d80:                                     000284d0 800db6ac 805fc564 bc14c580

7da0: 00000000 7effffee 80608d60 bfe73d40 bfe73d40 bff147fc 00000000 800db6ac

7dc0: 00000000 bc14c580 7effe000 7effffee 7effffee bc0b5fb8 bff147fc 800d88b4

7de0: 00000000 00000000 00000000 bc14c580 7effffee 7effffee bc0b5fb8 800d47b0

7e00: 805fbb40 00000001 00000000 8009228c 8c010e40 bc0b5fb8 bfe73d40 60000113

7e20: bfe73d40 8bffe280 00000000 bc0b5fb8 bfe73d40 bc0b4000 000003f7 7effffee

7e40: bfe73d40 bc14c580 bc0b5fb8 00000001 00000000 800d4954 bc0b5fb8 00000001

7e60: 00000000 00000017 bc14c580 bfd472c0 7effffee bfe73d40 00000000 bff0a700

7e80: 00000000 800d4bd0 bc026000 00000000 00000001 00000020 00000000 bc027edc

7ea0: 00000080 00000001 bff0a700 bc026000 00000000 bc026000 00000000 bff0a700

7ec0: bff0a7b0 800f0088 00000017 bc027edc 00000000 00000000 8045b960 bc00a3c8

7ee0: 00000080 0000000e 00000ffc 0000000e 7effffee 800f0248 bc00a3c0 00000000

7f00: 805e222e 00000000 00000000 00000000 bffef000 bc026000 00000000 bffef000

7f20: 00000001 bff0a700 bc026000 bc027f78 bc00a3c0 800f037c 00000000 00000080

7f40: bff8bc3c 800f1174 bc026000 00000000 805c3cc0 bff8bc3c 805e2220 bc027f78

7f60: bffef000 00000000 00000000 00000000 00000000 80043024 00000000 00000000

7f80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

7fa0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

7fc0: ffffffff bfeaccc0 bff894e0 00000000 ffffffff 00000000 00000000 80085b28

7fe0: 00000000 bfeaccc0 80085a2c 80040a18 00000013 80040a18 67a118f5 60833196

[<800e7678>] (kmem_cache_alloc+0xd4/0x110) from [<800db6ac>] (anon_vma_prepare+0x2c/0x168)

[<800db6ac>] (anon_vma_prepare+0x2c/0x168) from [<800d88b4>] (expand_downwards+0x14/0x1a0)

[<800d88b4>] (expand_downwards+0x14/0x1a0) from [<800d47b0>] (handle_pte_fault+0x654/0x72c)

[<800d47b0>] (handle_pte_fault+0x654/0x72c) from [<800d4954>] (handle_mm_fault+0xcc/0x16c)

[<800d4954>] (handle_mm_fault+0xcc/0x16c) from [<800d4bd0>] (__get_user_pages+0x124/0x2f0)

[<800d4bd0>] (__get_user_pages+0x124/0x2f0) from [<800f0088>] (get_arg_page+0x50/0xb4)

[<800f0088>] (get_arg_page+0x50/0xb4) from [<800f0248>] (copy_strings+0x15c/0x270)

[<800f0248>] (copy_strings+0x15c/0x270) from [<800f037c>] (copy_strings_kernel+0x20/0x28)

[<800f037c>] (copy_strings_kernel+0x20/0x28) from [<800f1174>] (do_execve+0x1ac/0x268)

[<800f1174>] (do_execve+0x1ac/0x268) from [<80043024>] (kernel_execve+0x38/0x7c)

[<80043024>] (kernel_execve+0x38/0x7c) from [<80085b28>] (____call_usermodehelper+0xfc/0x124)

[<80085b28>] (____call_usermodehelper+0xfc/0x124) from [<80040a18>] (kernel_thread_exit+0x0/0x8)

Code: 1affffe9 e5948014 e28bb004 e3a0c001 (e7968008)

---[ end trace 86a7da615f57aaee ]---

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd

Unable to handle kernel paging request at virtual address 10446000

But when i use the Mfgtools-Rel-3.0.0_20121119_GA_MX6Q_UPDATER to download android 4.04 prebuilt image, it succeed

Is it that  my board is too old to may it happen?

Labels (2)
0 Kudos
Reply
2 Replies

613 Views
SergioSolis
NXP Employee
NXP Employee

you should be able to download the latest android to that revision of the board without problems. What profile are you using to download it?, I have tried EMMC without issues.

0 Kudos
Reply

613 Views
soursunny
Contributor II

[profiles]

chip = MX6Q Linux Update

[platform]

board = SabreSD

[LIST]

name = Android-SabreSD-EMMC

0 Kudos
Reply