Mfgtool can't connect in windows7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mfgtool can't connect in windows7

6,419 次查看
yongkimin
Contributor III

Hi all,

I can't connect in windows 7 pc, but connection in windows xp is ok.

When Mfgtool try connect in win 7 the HID(human interface device) interrupt does not occur in control panel.

Anyone there tell me the why?

Thanks.

标签 (1)
0 项奖励
回复
7 回复数

3,262 次查看
Yuri
NXP Employee
NXP Employee

There is  a problem with USB3 options, when using loader / tools, using serial (USB) i.MX bootloader(s). 

For example, some MFG problems relate to the general USB3 support under OS and issues may be solved,

when USB3 ports are disabled in Win 7 / 8. Please try to disable USB3 if possible.   

I expect MFG tool, supporting USB3, will be published soon.


In meantime You may try one of preliminary (non-published) MFG release, supporting USB3.

Let me know if needed. 

0 项奖励
回复

3,262 次查看
yongkimin
Contributor III

Thanks Yuri.

First, the problem is not USB3. Sorry my mistakes to describe the my problem.

My problem is can't connect the USB2 to Win 7 PC on USB boot mode. In Win XP I can connect the my board with USB2 cable. In control panel of win xp pc reports the HID device was connected when I connect the USB2 cable.

So I can't use mfgtool in win 7 pc. I guess my board is something different USB2 connection with imx28 evk.

Thanks.

0 项奖励
回复

3,262 次查看
Yuri
NXP Employee
NXP Employee

You may try the enclosed

0 项奖励
回复

3,262 次查看
nico70
Contributor I

Dear Yuri,

I'm search a source code for the mfgtool version 1.6.2.0055.

would you have a link?

0 项奖励
回复

3,262 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复

3,262 次查看
Yuri
NXP Employee
NXP Employee

You may try the enclosed

0 项奖励
回复

3,262 次查看
Yuri
NXP Employee
NXP Employee

I tried the MFG under Windows 8 : at least the i.MX28 HID was detected after removing USB3.

Re: Windows 8.1 preview and i.MX28

0 项奖励
回复