MfgTool image downloading error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MfgTool image downloading error

Jump to solution
2,101 Views
xhlow
Contributor II

Hi All,

I just received a MCIMX6ULL-EVK this week. I tried to download image using MfgTool2 with  L4.9.88_2.0.0 iMX6,7 BSP. But it show error message below when I downloading the image.

 
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (May 01 2018 - 15:03:05 -05 00)

CPU: Freescale i.MX6ULL rev1.0 at 396 MHz
Reset cause: POR
Model: Freescale i.MX6 ULL DDR3 ARM2 Board
Board: MX6ULL 14X14 DDR3 ARM2
DRAM: 1 GiB
ERROR: read error from device: bef4a9a8 register: 0x0!
at /home/bamboo/build/4.9.X-2.X/fsl-imx-xwayland/temp_build_dir/build_fsl-imx-xw ayland/tmp/work/imx6ull14x14ddr3arm2-poky-linux-gnueabi/u-boot-imx/2017.03-r0/gi t/drivers/power/pmic/pfuze100.c:46/pfuze100_read()
Not supported, id=11
initcall sequence bffa8920 failed at call 878042d4 (err=-22)
### ERROR ### Please RESET the board ###

Kindly need your help on this?

Thanks.

Regards,

XH Low

Labels (4)
0 Kudos
Reply
1 Solution
1,821 Views
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

View solution in original post

0 Kudos
Reply
4 Replies
1,822 Views
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

0 Kudos
Reply
1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi XH Low

from log it is not MCIMX6ULL-EVK but "MX6ULL 14X14 DDR3 ARM2" and it has

different uboot image:

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,821 Views
xhlow
Contributor II

Hi Igor,

May I know where to get this u-boot image? 

Thanks.


Regards,

XH Low

0 Kudos
Reply
1,821 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply