Mfg tool for imx6sl emmc flash - Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mfg tool for imx6sl emmc flash - Yocto

Jump to solution
1,475 Views
karthikeyanraju
Contributor III

Hi,

I m using iMX6SL-evk board. I want flash Yocto 4.9.88 images into EMMC.

I have downloaded L4.9.88_2.0.0-ga_mfg-tools.tar.gz mfg tool.

This is having with rootfs and without rootfs tools. I want to flash with rootfs.

I could not find VBS file related to my requirement.

Which is the perfect VBS file to flash yocto images into iMX6sl-evk EMMC device ?

Please provide me the guidance.

Thanks.

Labels (2)
0 Kudos
Reply
1 Solution
1,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karthikeyan

i.MX6SL EVK has not emmc populated and it is connected to the same usdhc port

as sd, so there is no appropriate vbs script for it. One can try mfgtool2-yocto-mx-evk-emmc.vbs

and changing ucl2.xml and adding for LIST name="eMMC" codes for ifdev="MX6SL".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,297 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karthikeyan

i.MX6SL EVK has not emmc populated and it is connected to the same usdhc port

as sd, so there is no appropriate vbs script for it. One can try mfgtool2-yocto-mx-evk-emmc.vbs

and changing ucl2.xml and adding for LIST name="eMMC" codes for ifdev="MX6SL".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply