Methods to allocate EBA for IDMAC in IPU

cancel
Showing results forย 
Search instead forย 
Did you mean:ย 

Methods to allocate EBA for IDMAC in IPU

Jump to solution
164 Views
pradeepasenanay
Contributor II

Hello,

In the Linux kernel source the EBA for IPU-CPMEM is allocated using the dma_alloc_coherent API. Is this a must to do?

I'm writing a driver from the scratch for a very specific CSI module manipulation and therefore I would like to know whether there are any other ways to perform this memory allocation (ie. kmalloc).

In SDK the memory used for the EBA is,

#define IPU_DMA_MEMORY_START0x40000000

#define CH0_EBA1(IPU_DMA_MEMORY_START + 0x01C00000)

Do these memory locations have any special attributes associated or can I use any memory location by allocating through kmalloc?

Can someone give me some thought for this?

Thank you in advance.

Pradeepa

Labels (2)
0 Kudos
1 Solution
52 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Pradeepa

any memory location can be used but

IPU IDMAC can operate only with unfragmented memory,

so seems one can use kmalloc, but verify that requirement.

EBA is described in sect.37.4.2.7 IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
53 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Pradeepa

any memory location can be used but

IPU IDMAC can operate only with unfragmented memory,

so seems one can use kmalloc, but verify that requirement.

EBA is described in sect.37.4.2.7 IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos