Merge weston patch related to hdmi unplug/replug and fullscreen mode lost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Merge weston patch related to hdmi unplug/replug and fullscreen mode lost

841 Views
vix
Contributor II

Upstream weston developers just merged this patch, so that weston doesn't loose fullscreen mode if the HDMI cable is unplugged and then plugged again (see here).

Since the issue has been reported on a iMX8M processor, can NXP merge this pacth in its own weston fork (that O think is this one, but I can be wrong)?

Thanks

0 Kudos
6 Replies

767 Views
vix
Contributor II

Hi @Sanket_Parekh 

probably my previous answer got lost somewhere.

I don't use a BSP fro NXP, but TorizonCore from Toradex. And Toradex said it's based on NXP fork of weston.

I don't think it's already included, because the mainteners of weston added the patch some days ago (based on the issue I created).

And, in any case, I think it's easy for one of the NXP developers, checking if the patch is included or not.

Can you ask someone to verify, please?

 

0 Kudos

751 Views
vix
Contributor II

I received some email with answers from @Sanket_Parekh but I can't see them here.

The emails contain a link to the community, but it points to a non-existing page.

What is wrong?

0 Kudos

687 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @vix 

Please find the response of the engineering team below.

I have checked the latest version of weston-imx-11.0.1, the patch hasn't been added.

weston_image.jpeg

 

Thanks & Regards,

Sanket Parekh

 

0 Kudos

679 Views
vix
Contributor II

Hi @Sanket_Parekh 

I cannot see the answer from the engineering team.

0 Kudos

806 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @vix ,

I hope you are doing well.

I have a query to ask, Please find it as given below.

->Which Linux BSP are you using?
->Please check whether the patch you are merging is included in the latest BSP or not.
->If not then One has to wait for the next quarter's release for the same.
->If yes then please use the latest Linux BSp for the same.

Thanks & regards,

Sanket Parekh

0 Kudos

771 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @vix ,

I hope you are doing well.

Any Update on this from your side?

Thanks & Regards,

Sanket Parekh

0 Kudos