Memory size of HiFi4 Core on i.MX 8M Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Memory size of HiFi4 Core on i.MX 8M Plus

跳至解决方案
1,710 次查看
StXue
Contributor I

Hello,
I have some doubts about the memory size of HiFi4 Core.

In memory map of Context-A53 and Context-M7, I found a same region "Audio DSP" memory bus address form 3B00_0000 to 3BFF_FFFF 16MB. Is this the shared memory between multiple cores?

But in memory map of HiFi4, most of them are reserved, like 3B77_0000 3BFF_FFFF. 

Does it mean on HiFi4, we only have 256KB OCRAM_A and 64KB DTCM memory can be used?

Because on MX RT685, I can assign more memory to DSP Core, from ARM side.

Look forward to your favourable reply, thanks!

0 项奖励
回复
1 解答
1,699 次查看
joanxie
NXP TechSupport
NXP TechSupport

the Linux OS kernel reserves the memory for the DSP in the SDRAM separately. The range of the reserved
memory is 0x92400000 ~ 0x943fffff (32 MB). You may set this reserved memory by changing the imx8mp.dtsi file in the

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?..."

reserved-memory {
…………….
dsp_reserved: dsp@92400000 {
reg = <0 0x92400000 0 0x1000000>;
no-map;
};
dsp_reserved_heap: dsp_reserved_heap {
reg = <0 0x93400000 0 0xef0000>;
no-map;
};
dsp_vdev0vring0: vdev0vring0@942f0000 {
reg = <0 0x942f0000 0 0x8000>;
no-map;
};
dsp_vdev0vring1: vdev0vring1@942f8000 {
reg = <0 0x942f8000 0 0x8000>;
no-map;
};
dsp_vdev0buffer: vdev0buffer@94300000 {
compatible = "shared-dma-pool";
reg = <0 0x94300000 0 0x100000>;
no-map;
};

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,696 次查看
StXue
Contributor I

Thank you for your support.

0 项奖励
回复
1,700 次查看
joanxie
NXP TechSupport
NXP TechSupport

the Linux OS kernel reserves the memory for the DSP in the SDRAM separately. The range of the reserved
memory is 0x92400000 ~ 0x943fffff (32 MB). You may set this reserved memory by changing the imx8mp.dtsi file in the

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?..."

reserved-memory {
…………….
dsp_reserved: dsp@92400000 {
reg = <0 0x92400000 0 0x1000000>;
no-map;
};
dsp_reserved_heap: dsp_reserved_heap {
reg = <0 0x93400000 0 0xef0000>;
no-map;
};
dsp_vdev0vring0: vdev0vring0@942f0000 {
reg = <0 0x942f0000 0 0x8000>;
no-map;
};
dsp_vdev0vring1: vdev0vring1@942f8000 {
reg = <0 0x942f8000 0 0x8000>;
no-map;
};
dsp_vdev0buffer: vdev0buffer@94300000 {
compatible = "shared-dma-pool";
reg = <0 0x94300000 0 0x100000>;
no-map;
};

 

0 项奖励
回复