Memory configuration for i.MX8QXP in U-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory configuration for i.MX8QXP in U-boot

4,559件の閲覧回数
Maddis
Contributor IV

Hi,

I'm trying to find lpddr4 configuration for imx8qxp-mek -development board from U-boot, but either it's not there or I'm blind because I just can't seem to find it. There is one for imx8m, but that is different CPU and it's not being used. Seems that imx8qxp_mek_config - file is being used.

I see that imx8m devicetree blobs are being generated, but I haven't yet been able to find which one of them are being used (if any at u-boot). 

On i.MX6 it was easy since ddr timing was set at board-configuration file, but not so much no i.MX8 it seems.

Where I can find the lpddr4 config for i.MX8qxp-mek - board in U-boot? U-boot version seems to be u-boot-imx-2017.03.

0 件の賞賛
返信
10 返答(返信)

3,297件の閲覧回数
_angelo_
Contributor III

But imx8qxp mek i have here, B0, uses 

MT53B768M32D4DT-062
LPDDR4 24G 768MX32 (3GB) 1.6 GHz

And ddr init in the scfw porting kit seems for 1.2Ghz (imx8qx_dcd_1.2GHz.cfg).

Why ?

 

 

 

0 件の賞賛
返信

3,984件の閲覧回数
simon_ko
Contributor III

Hi Joan.

I also want to configure LPDDR4 with i.mx8qxp.
Can I receive the setting excel file?

0 件の賞賛
返信

3,984件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

3,984件の閲覧回数
simon_ko
Contributor III

Hi joan.

I got the Excel configuration file from NXP Korea.

Thank you for your support.

0 件の賞賛
返信

3,984件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I will mail "i.MX8QXP Validation And MEK LPDDR4 Register Programming Aids" to you

3,984件の閲覧回数
danwright
Contributor I

Hi Joan-

This might be exactly what I'm looking for too...  can you send these to me as well?  It does not appear that any code of this description is to be found for download...

Thanks!

Dan

0 件の賞賛
返信

3,984件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

dwright@cumminsallison.com is this your mail address?

0 件の賞賛
返信

3,984件の閲覧回数
danwright
Contributor I

No- my email address is:  dan.wright@chargepoint.com.  But I have since convinced myself that the initialization of the DDR is actually in the SCU code.  And I have found this initialization in the imx-scfw-porting-kit-1.2.5 code.

0 件の賞賛
返信

3,984件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

OK, since you have already figure this out , I don't send any mail to you for this question

0 件の賞賛
返信

3,984件の閲覧回数
Maddis
Contributor IV

Hi,

This was exactly I was looking for. Thanks!

0 件の賞賛
返信