Memory allocation in MIMXRT1176 via MCUXpresso IDE v11.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory allocation in MIMXRT1176 via MCUXpresso IDE v11.

1,136件の閲覧回数
mike2000
Contributor I

Hello.

In the process of working with the MIMXRT1176 processor, I had a need to reallocate the TCM memory, subtract 48 kB from the ITCM area and add them to the DTCM area. I reviewed document "AN12077 Using the i.MX FlexRAM", but there is an example for IAR.

  1. Tell me, where can I get more information on memory allocation through MCUXpresso IDE, which document should I refer to?
  2. How to use OCRAM1/2 memory via MCUXpresso IDE? When building a project, all arrays are placed in DTCM memory by default. I need to place some arrays in OCRAM memory, because they all do not fit in DTCM.
ラベル(3)
0 件の賞賛
返信
1 返信

1,130件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信