Memory access of I.MX6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Memory access of I.MX6q

跳至解决方案
1,679 次查看
aishashaik
Contributor II

1.Do user can access the secure  RAM(internal) memory ?

2. which area of ROM can user access?

3.How to flash the user developed firmware in the internal ROM?

4.As a part of secure boot how user can flash public key in the internal ROM? is it the location is OTP?

5.Any tool is required for the above? if yes please share the details?

标签 (2)
1 解答
1,534 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aisha

keys are contained in OTP. For other questions

please refer to Security Manual

https://community.freescale.com/docs/DOC-97660

AN4581 Secure Boot

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0291.pdf

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,535 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aisha

keys are contained in OTP. For other questions

please refer to Security Manual

https://community.freescale.com/docs/DOC-97660

AN4581 Secure Boot

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0291.pdf

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,534 次查看
aishashaik
Contributor II

Thank you igorpadykov for your quick reply

0 项奖励
回复