Memory access of I.MX6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory access of I.MX6q

ソリューションへジャンプ
1,690件の閲覧回数
aishashaik
Contributor II

1.Do user can access the secure  RAM(internal) memory ?

2. which area of ROM can user access?

3.How to flash the user developed firmware in the internal ROM?

4.As a part of secure boot how user can flash public key in the internal ROM? is it the location is OTP?

5.Any tool is required for the above? if yes please share the details?

ラベル(2)
1 解決策
1,545件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aisha

keys are contained in OTP. For other questions

please refer to Security Manual

https://community.freescale.com/docs/DOC-97660

AN4581 Secure Boot

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0291.pdf

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,546件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aisha

keys are contained in OTP. For other questions

please refer to Security Manual

https://community.freescale.com/docs/DOC-97660

AN4581 Secure Boot

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0291.pdf

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,545件の閲覧回数
aishashaik
Contributor II

Thank you igorpadykov for your quick reply

0 件の賞賛
返信