Media clock synchronisation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Media clock synchronisation

1,040 Views
mythilir
Contributor I

Hi,

  I am trying to adjust the pll of my audio codec sgtl5000. But I dont find any interface like ioctl or gpio or alsa api through which the adjustment can be done. Can anyone suggest how pll syntonisation can be achieved. This required for my media clock synchronization between two nodes.

0 Kudos
Reply
1 Reply

959 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mythili

these apis or ioctl are not implemented in code

you should write them himself.

Also not sure if pll syntonisation can be achieved at all.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply