Measure ADC of PWM signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Measure ADC of PWM signal

跳至解决方案
2,995 次查看
emdev
Contributor III

Hello,

I want to read ADC value of PWM signal.

ADC values are changed.

If read ADC value at lowest value of PWM, it report 0.

But if read ADC value at highest value of PWM, it report Vcc.

I can check MPC5643L_PWM_ADC_concept.pdf and find below image.

emdev_0-1635404275434.png

I want to read ADC at highest value of PWM.

How I can approach it?

Duty cycle of PWM can be changed.

Thanks in advance.

 

 

标签 (1)
0 项奖励
回复
1 解答
2,992 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

 

one can read several samples (the more number, the better accuracy) then compare them in

software and select one with highest value.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,982 次查看
emdev
Contributor III

Hi igorpadykov,

I used methods which you recommended and it works well.

But I want to check that there are any hardware or chipset level solutions or not?

For example, DMA or automatic method in https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5643L-PWM-ADC-measurement-concept/ta-p/110265....

If there is no other chipset level methods, I'll use method which you recommended.

Thanks.

0 项奖励
回复
2,980 次查看
igorpadykov
NXP Employee
NXP Employee

> I want to check that there are any hardware or chipset level solutions or not?

 

sorry there are no hardware solutions for such task.

 

Best regards
igor

0 项奖励
回复
2,993 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

 

one can read several samples (the more number, the better accuracy) then compare them in

software and select one with highest value.

 

Best regards
igor

0 项奖励
回复