Meaning of "Pull Resistor Enable Field" at Config Tools for i.MX v9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Meaning of "Pull Resistor Enable Field" at Config Tools for i.MX v9

Jump to solution
1,708 Views
sergiospader
Contributor II

Good Morning,

A simple question, at Config Tools for i.MX v9, one of the options to configure a GPIO is "Pull Resistor Enable Field", what is the exact meaning of this option ? Can you also verify if the other options I understand correctly (see below) ?

Pull-Up Enable Field - Include a Pull-up at internal PAD works for Input and Output.

Software Input on Field - Read the PAD in a Output GPIO, wors for Output only

Hysteresis Enable Field -  Hysteresis the input signal, works for input only

Open Drain Enable Field - Open Drain Output,  works for Output only

Slew rate Field - Output slew rate - works for Output only

Drive Strenght Field - Output Drive Strength -  works for Output only

Thanks

0 Kudos
1 Solution
1,700 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

your understanding is correct except SION (Software Input on Field) - it works

for Input and Output. Also may be useful AN5078

Influence of Pin Setting on System Function and Performance

 

Best regards
igor

View solution in original post

0 Kudos
7 Replies
1,701 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

 

your understanding is correct except SION (Software Input on Field) - it works

for Input and Output. Also may be useful AN5078

Influence of Pin Setting on System Function and Performance

 

Best regards
igor

0 Kudos
1,687 Views
sergiospader
Contributor II

Hello Igor,

Thanks for Quick answer.

How about the  "Pull Resistor Enable Field" ? As the Pull-Up resistor is another field, what is the meaning of this "Pull Resistor Enable Field" ?

At the .c this option is the "PE:" as below:

- {pin_num: AB9, peripheral: GPIO1, signal: 'gpio_io, 15', pin_signal: GPIO1_IO15, PE: Disabled}

Thanks

0 Kudos
1,683 Views
igorpadykov
NXP Employee
NXP Employee

>How about the "Pull Resistor Enable Field" ? 

 

your understanding is correct:

"Pull-Up Enable Field - Include a Pull-up at internal PAD works for Input and Output."

 

Best regards
igor

 

 

 

 

0 Kudos
1,680 Views
sergiospader
Contributor II

Igor,

look the attached picture, there is two different fields 

"Pull Resistors Enable Field"

"Pull Up Enable Field"

one generate in .c "PE: " and the other "PUE:" as below:

- {pin_num: AG10, peripheral: GPIO1, signal: 'gpio_io, 08', pin_signal: GPIO1_IO08, identifier: RTC_INT_N, direction: INPUT, PE: Enabled, PUE: Enabled, SION: DISABLED,
HYS: Enabled, FSEL: SLOW0, DSE: X1_0}

The Pull-up I understand, I wan't to understand what is the "Pull Resistors Enable Field"

Sérgio

 

 

0 Kudos
1,674 Views
igorpadykov
NXP Employee
NXP Employee

>I wan't to understand what is the "Pull Resistors Enable Field"

 

1.jpg

 

Best regards
igor

0 Kudos
1,668 Views
sergiospader
Contributor II

Hello Igor, thanks for the answer.

For me it is not clear yet... I had seen this table... let me try to explain.

Is this register a "global Pull configuration" ? Then if this register is disable the Pull-Up register next is don't care ?

Or it is a Pull-Down enable Register ? Or Other thing.... the sentence: "Pull Resistor Enable Field" is too vage

And it is valid for input or output ?.... I wan't to understand what is physically happen when I enable this register...

Thanks

 

 

0 Kudos
1,666 Views
igorpadykov
NXP Employee
NXP Employee

>Is this register a "global Pull configuration" ?

yes

 

>And it is valid for input or output ?

for both

 

Best regards
igor

0 Kudos