Meaning of fslc acronym?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Meaning of fslc acronym?

ソリューションへジャンプ
5,129件の閲覧回数
paolosantini
Contributor III

Trivial question: "fslc" found in document (example: ...The i.MX Yocto Project Community BSP uses u-boot-fslc from the mainline,...) what does it stand for?

It seems to be FileSystem..lc ??? Or whatelse?

Thanks in advance

Paolo

ラベル(1)
0 件の賞賛
返信
1 解決策
5,057件の閲覧回数
gary_bisson
Senior Contributor III

Hi Paolo,

FSL means Freescale as those repositories and the CPU it supports existed before NXP bought Freescale.

And 'C' means Community. So all fslc repositories you see are maintained and updated by the community.

Hope this helps.

Regards

Gary

元の投稿で解決策を見る

2 返答(返信)
5,058件の閲覧回数
gary_bisson
Senior Contributor III

Hi Paolo,

FSL means Freescale as those repositories and the CPU it supports existed before NXP bought Freescale.

And 'C' means Community. So all fslc repositories you see are maintained and updated by the community.

Hope this helps.

Regards

Gary

5,057件の閲覧回数
paolosantini
Contributor III

Thanks Gary, very useful.

BR

Paolo

0 件の賞賛
返信