May unused USB OTG pins be connected to ground?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May unused USB OTG pins be connected to ground?

794 Views
frankambrosius
Contributor II

As clearly stated in the HDG, the unused USB OTG pins should be left floating when unused.

However, I need them (OSB_OTG_DN and DP) to be connected to ground. Is this allowed? What are the consequences of doing this?

Thank for all the help!

Regards,

Frank

Labels (2)
0 Kudos
Reply
3 Replies

692 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

yes they can be connected to ground, with consequences

of small leakage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

692 Views
frankambrosius
Contributor II

Hi Igor,

Thank you for your reply.

Can you also indicate how much the leakage current will be?

Is this specified in the datasheet?

Regards,

Frank

0 Kudos
Reply

692 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

I am afraid this was not measured, however

it is small current.

Best regards

igor

0 Kudos
Reply