May I not populate PF0100 F0 SWBST components?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

May I not populate PF0100 F0 SWBST components?

ソリューションへジャンプ
1,641件の閲覧回数
MehmetAliIpin
Contributor V

Dear Sir/Madam,

Hello,

We have a project with I.MX6 dual/quad core processor which we use PF0100 F0 as PMIC. For USB I have another 5 volts supply already and therefore I don't want to populate SWBST components in PCB. Does it cause stability problems to PF0100 F0?

Thanks and best regards.

Mehmet Ali

タグ(2)
1 解決策
1,511件の閲覧回数
durmus
Contributor IV

Hi Mehmet Ali,

You should check out the following document:

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

For every pin, there is a column for "Recommended connection when not used".

For your specific question, it says in the document:

44 - SWBSTFB --> Leave floating

45 - SWBSTIN --> Connect to VIN

46 - SWBSTLX --> Leave floating

Best regards,

Durmuş

元の投稿で解決策を見る

2 返答(返信)
1,512件の閲覧回数
durmus
Contributor IV

Hi Mehmet Ali,

You should check out the following document:

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

For every pin, there is a column for "Recommended connection when not used".

For your specific question, it says in the document:

44 - SWBSTFB --> Leave floating

45 - SWBSTIN --> Connect to VIN

46 - SWBSTLX --> Leave floating

Best regards,

Durmuş

1,511件の閲覧回数
MehmetAliIpin
Contributor V

Thank you,

I found and read AN4717 after I asked the question.

Best regards.

Mehmet Ali

0 件の賞賛
返信