Maximum operating clock of iMX535 vs ambiant temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum operating clock of iMX535 vs ambiant temperature

557 Views
Lorac
Contributor III

We have some part availability issue with NXP part number MCIMX535DVV2C
that we operate at 1.2GHz.
My question is: If we operate this processor at maximum 70C by design,
can we use also MCIMX535DVV1C even if this part was
specified for 1GHz at 95C?

Thanks
CD

Labels (1)
0 Kudos
1 Reply

544 Views
Yuri
NXP Employee
NXP Employee

@Lorac 
Hello,

   MCIMX535DVV1C  has not been specified and tested for 1.2 MHz,
therefore we cannot guarantee proper operations under 1.2 MHz.

  Customers can use now MCIMX535DVP2C2 1.2 GHz

Regards,
Yuri

0 Kudos