Maximum memory capacity of iMX8M PLUS SoC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum memory capacity of iMX8M PLUS SoC

716 Views
feyzaboztepe
Contributor I

Hello ,

What is the maximum memory capacity that will support iMX8M PLUS SoC ?

 

0 Kudos
Reply
3 Replies

667 Views
feyzaboztepe
Contributor I

Hello , 

Well , How much memory is required for eMMC? 

0 Kudos
Reply

636 Views
Oswalag
NXP TechSupport
NXP TechSupport

I hope you are doing well,

The iMX8MP supports eMMC Flash 5.1, which means all of the eMMCs of this generation (5.1) are supported.
The eMMC is a serial memory and should be not a problem with the capacity as long as the memory meets the requirements of the processor.

Have a nice day!!

0 Kudos
Reply

677 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello, 

The max lpddr4 and ddr4 is 8Gbyte.

Regards.

0 Kudos
Reply