Maximum memory capacity of iMX8M PLUS SoC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum memory capacity of iMX8M PLUS SoC

767 次查看
feyzaboztepe
Contributor I

Hello ,

What is the maximum memory capacity that will support iMX8M PLUS SoC ?

 

0 项奖励
回复
3 回复数

718 次查看
feyzaboztepe
Contributor I

Hello , 

Well , How much memory is required for eMMC? 

0 项奖励
回复

687 次查看
Oswalag
NXP TechSupport
NXP TechSupport

I hope you are doing well,

The iMX8MP supports eMMC Flash 5.1, which means all of the eMMCs of this generation (5.1) are supported.
The eMMC is a serial memory and should be not a problem with the capacity as long as the memory meets the requirements of the processor.

Have a nice day!!

0 项奖励
回复

728 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello, 

The max lpddr4 and ddr4 is 8Gbyte.

Regards.

0 项奖励
回复