Hi all,
Is there any data of maximum force for heat-sink attachment ?
We'll plan to use i.MX8M Mini and found data for some body sizes in 6.2 of following doc.
However, there are no data for 14 x 14 mm like i.MX8M Mini and Nano.
https://www.nxp.com/docs/en/application-note/AN4871.pdf
Could you provide the maximum force for 14 x14 mm package ?
Ko-hey
Solved! Go to Solution.
NXP recommends that the maximum load force not exceed 10 lbs (44 N).