Maximum display resolution of i.MX51 in dual display mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum display resolution of i.MX51 in dual display mode

705件の閲覧回数
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic: LCD, Display, IPU

 

Question.  What is maximum display resolution of i.MX51 in dual display mode ?

 

Answer.  Maximal peak rate (including blanking overhead) of i.MX51 :

- Single display: 110 MPixel/sec

- Total: 120 MPixel/sec

 

So, if SXGA (1280x1024 ~ 1.3 MP) is the first display, this consumes 78 MP/sec = 1.3MP * 60 Hz, therefore only additional WQVGA (400x240 ~ 96 KP, ~5.8MP/sec) display can be supported.

 

WVGA configuration (800x480 ~ 0.4 MP) exceeds performance restriction, since it consumes ~24MP/sec at 60Hz.

 

Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

タグ(1)
0 件の賞賛
返信
0 返答(返信)