Maximum Current consumption for NVCC in I.MXrt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum Current consumption for NVCC in I.MXrt

1,285 Views
Newton829
Contributor II

Hello, 

   In I.MXRT 117x , the current consumption is shown by 

Albert_Einstein_0-1689222318530.png

In I.mxRt series 

N= 16 no  of pins

V =  The operating voltage of NVCC i.e 3.3

But how to calculate C and F for the equation?

1.Is C the value of bypass capacitor, which we place near the pin or is it something else?

2. Is the F is the clock frequency given to the peripheral ? What the max-min value I must consider?

Thank you

 

Labels (2)
Tags (2)
0 Kudos
4 Replies

488 Views
Rajeswari
Contributor I

Hi,

I'm using i.MXRT1064 for one of my requirement. I need to calculate the current consumption for NVCC-EMC, SD0, SD1 and GPIO.

Mentioned CL is 3.8pF, but in datasheet this load capacitance value not mentioned anywhere in i.MXRT1064 datasheet. Please provide the reference for this capacitance value to calculate the required current.

0 Kudos

711 Views
Newton829
Contributor II

@Omar_Anguiano 

There is one more parameter in i.mx Rt datasheet called as IOCT which 100mA.

Albert_Einstein_0-1691736083985.png

1.Does this parameter has relation with NVCC?

2.Can I consider this as maximum rating of NVCC line?

3.Please help me understand what this parameter mean?

 

Thank you,

Regards

0 Kudos

686 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

1. Yes, a bank is the group of pins supplied by a specific NVCC line, e.g. NVCC_EMC_B1.
2. Correct. To be more complete the maximum current of the IOs from a bank.

Best regards,
Omar

0 Kudos

1,256 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello I hope you are well.

The C value depends on what you have connected to the GPIO pins. This is a value that varies depending on the specific application. F states for the GPIO toggle rate.
You might use the datasheet CL value from the IO parameters.

I will share with you an example from a SEMC calculation taking 16bit SEMC+IS42S83200B @166M as an example.

Omar_Anguiano_0-1689362710755.png

 

Imax=16 x 3.8pF x 3.3v x (0.5x166MHz)  = 16mA.  

It can evaluate the IO power consumption by this formula, however, only CLK signals can reach to 166Mhz, other data signals don't have this high frequency, so this is a rough evaluation for IO power consumption, anyway, you can use this calculation as a approximative evaluation.

Best regards,
Omar

0 Kudos