I want to use https://www.nxp.com/design/designs/nxp-edgeready-mcu-based-solution-for-face-recognition-with-livene... this board for development of facial recognition product that should be able to detect face from a pool of 1000 faces. I checked the documentation but can not find the maximum number of faces supported by the kit. @nxp pls support for the same
Does the structure of code needs to be updated? Or hardware also needs to be updated like the memory etc? Or the same hardware can work for 1000 faces and we just need to do minor tweaks for having 1000 faces?
Also is there any active support available for development?
Hello,
The demo is able to show 100 faces, You need modify the code for 1000 faces.
Regards