Max RAM can be used from M4 in IMX7ULP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max RAM can be used from M4 in IMX7ULP

1,033 Views
vivekrajpara
Contributor III

Hello,

I am trying to find how much max memory can be used in Cortex M4 of IMX7ULP in Low power mode.

As I see from the ref manual, it seems that max 256KB can be used from internal RAM. 

Can someone please help to figure out if there is way to increase this RAM on M4 side?

Is there a way to access DDR conneted with A7 from M4 while keeping A7 in sleep mode?

Thanks in advance,

Regards,

Vivek

Labels (2)
3 Replies

939 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vivek,

For internal RAM are 256KB, for DDR you have only 2MB that are reserved for run Linux  the rest you can use with M4.

Regards

939 Views
vivekrajpara
Contributor III

Thanks for the reply.

 I am not able to find any project in M4 SDK which is accessing DDR section.

For most of the projects, linker script is pointing to Internal RAM / QSPI flash, can you please let me know if there is any project present in M4 SDK which is using DDR memory? It would be helpful for us to see method for accessing DDR from M4. It would be great if you can point to any document / sample which describes the method for accessing DDR from M4

Regards,

Vivek

0 Kudos

939 Views
vivekrajpara
Contributor III

Hi Bio_TICFSL‌,

Did you get a chance to look into this further query, it would be helpful if you can share the sample code for the same?

Regards,

Vivek

0 Kudos