Max OSPI memory in iMx8 Quad Max

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max OSPI memory in iMx8 Quad Max

ソリューションへジャンプ
1,279件の閲覧回数
ajmalmali
Contributor II

Hi

We are in the process of Processor analysis for a project. iMx8 Quad max is one of the major contenders. What is the max OSPI flash supported in iMx8QM. We see chips for up to 2Gb. Will this be supported in iMx8?

Regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,275件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,276件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信