Mask Set Errata for Mask 3N09P ID No. e9165

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mask Set Errata for Mask 3N09P ID No. e9165

ソリューションへジャンプ
713件の閲覧回数
goto11
Contributor III

Hello,Community

There is a description of “eCSPI: TXFIFO empty flag glitch can cause the current FIFO transfer to be sent twice”.
Is this description not applicable to Quad Serial Peripheral Interface (QuadSPI)?

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
638件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

right, it is not applicable to QuadSPI module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
639件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

right, it is not applicable to QuadSPI module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信