Marvell Wi-Fi chip not powering up sometimes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Marvell Wi-Fi chip not powering up sometimes

596件の閲覧回数
abrafo78777
Contributor I

Marvell Wi-Fi chip not powering up sometimes, need a power cycle to fix it.

When not working can see the below kernel logs:

[ 33.761628] wifi_pwrdn_fake_regulator: disabling
[ 33.766796] pcie_switch: disabling

When working can see the below kernel logs:

[ 6.890983] mwifiex_pcie 0000:01:00.0: enabling device (0000 -> 0002)

[ 6.891185] mwifiex_pcie: PCI memory map Virt0: (____ptrval____) PCI memory map Virt2: (____ptrval____)
[ 7.981533] mwifiex_pcie 0000:01:00.0: info: FW download over, size 634228 bytes
[ 8.746214] mwifiex_pcie 0000:01:00.0: WLAN FW is active
[ 8.792578] mwifiex_pcie 0000:01:00.0: Unknown api_id: 3
[ 8.799423] mwifiex_pcie 0000:01:00.0: Unknown api_id: 4
[ 8.806199] mwifiex_pcie 0000:01:00.0: Unknown GET_HW_SPEC TLV type: 0x217
[ 8.832063] mwifiex_pcie 0000:01:00.0: info: MWIFIEX VERSION: mwifiex 1.0 (16.68.1.p195)
[ 8.841397] mwifiex_pcie 0000:01:00.0: driver_version = mwifiex 1.0 (16.68.1.p195)

 

Using Apalis IMX8QM SOM with kernel version 5.4.77-5.1.0.

 

Is there any fix for this issue? Thanks in advance.

0 件の賞賛
返信
1 返信

589件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @abrafo78777!

Thank you for contacting NXP Support!

 

Are you using a custom base board?

The wifi that you want to use is that the SOM has or are you installing other wifi module?

 

What BSP version are you using?

 

Best Regards!

Chavira

0 件の賞賛
返信