Manufacturing tool not working on imx8 mek

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Manufacturing tool not working on imx8 mek

1,353 次查看
bi0h4z4rd
Contributor I

So, we are part of the Beta program for iMX8 and we own a imx8qxpmek board.

The Manufacturing tool that can be downloaded using the following link will NOT be able to detect, nor flash the board: https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.2.0_8QXP_Beta2_MFGTOOL&appType=license&locatio... 

While the one in the following link, works perfectly but is an older revision: https://www.nxp.com/webapp/Download?colCode=L4.9.51_MX8QX_Beta&appType=license&Parent_nodeId=1454108... 

Besides this, the kernel version that came in the SD (Linux imx8qxpmek 4.9.51-imx_4.9.51_8qm_beta1_8qxp_alpha+g33feef4 #1 SMP PREEMPT Sun Nov 12 09:58:43 CST 2017 aarch64 aarch64 aarch64 GNU/Linux) will support CAN0 and CAN1 (but not CAN2, but the version that i mention right above will have no CAN support at all (cannot bring up CANx as it says that dev does not exist).

It would be really appreciated if you could please fix BOTH issues.

Thanks!

Javier

0 项奖励
回复
2 回复数

1,092 次查看
art
NXP Employee
NXP Employee

Do you actually mean the i.MX8 or i.MX8X processor? What exactly board (exact part number) do you mean? Please specify.

0 项奖励
回复

1,092 次查看
shaohuili
Contributor I

I have a similar problem. It's i.MX8QXP processor.

0 项奖励
回复