Mag3110 Can't Receive the Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mag3110 Can't Receive the Interrupt

Jump to solution
1,141 Views
candywang
Contributor I

Mag3110 : The  INT PIN is high  all the time  after setting  it from  Standby to  Actived,So it can't receive the interrupt.

         Thanks & Best Regards

Labels (2)
0 Kudos
Reply
1 Solution
1,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Candy

4.4 not supported by nxp, please try official linux (4.1.15 or 4.9.x) releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor

View solution in original post

4 Replies
1,012 Views
candywang
Contributor I

Hi,Igor:

      It  is suitable for linux 2.6 kernel,but my linux kernel version is 4.4. It has received the interrupt all the time when i excuted "getevent" in the terminal,it is so surprised,the "getevent" is used for listening into the Real-time input message.

  Thank you very much

0 Kudos
Reply
1,013 Views
igorpadykov
NXP Employee
NXP Employee

Hi Candy

4.4 not supported by nxp, please try official linux (4.1.15 or 4.9.x) releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor

1,012 Views
candywang
Contributor I

Hi, Igor:

    Thank you very much! Best wishes to you ,Merry Christmas in advance!

0 Kudos
Reply
1,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Candy

one can look at Mag3110 example driver

MAG3110 3D Magnetic Sensor Full Feature Linux Driver for Smart Devices. (Rev 1) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply