MX8MP ISP with IR wavelengths

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8MP ISP with IR wavelengths

Jump to solution
1,268 Views
khang_letruong
Senior Contributor III

Dear ISP Experts,

When working with ISP, most of the use-cases are with visible light. However, I have a specific use-case of night-vision condition in which the scene would be illuminated with IR LED (850nm or 940nm) and supposing that the camera sensor has certain IR sensitivity, I would like to know if it is possible to calibrate the ISP in low-light condition but with IR illumination, please ?

Thanks in advance and best regards,
Khang

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,260 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, confirmed that we never tested this and couldn't guarantee this

 

View solution in original post

0 Kudos
Reply
1 Reply
1,261 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, confirmed that we never tested this and couldn't guarantee this

 

0 Kudos
Reply