MX8MP ISP with IR wavelengths

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX8MP ISP with IR wavelengths

ソリューションへジャンプ
787件の閲覧回数
khang_letruong
Senior Contributor III

Dear ISP Experts,

When working with ISP, most of the use-cases are with visible light. However, I have a specific use-case of night-vision condition in which the scene would be illuminated with IR LED (850nm or 940nm) and supposing that the camera sensor has certain IR sensitivity, I would like to know if it is possible to calibrate the ISP in low-light condition but with IR illumination, please ?

Thanks in advance and best regards,
Khang

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
779件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, confirmed that we never tested this and couldn't guarantee this

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
780件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, confirmed that we never tested this and couldn't guarantee this

 

0 件の賞賛
返信