MX8M :weston-simple-egl failed on debain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8M :weston-simple-egl failed on debain

1,719 Views
flyalfie
Contributor I

when I process weston-simple-egl.   the message is  "init_egl: Assertion `display->egl.dpy' failed". I saw the code is initEGL faild. it is work on the Yocto. but debain is failed.  please help me. thanks.

0 Kudos
Reply
5 Replies

1,601 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Chen,

You should download the latest BSP where weston compositor not failed however you can check with our third party if debian work with it:

https://developer.solid-run.com/knowledge-base/i-mx8m-debian/ 

https://boundarydevices.com/wiki/debian-for-nitrogen8/ 

Regards

0 Kudos
Reply

1,601 Views
flyalfie
Contributor I

I found out If I run the weston-simple-egl on the debian Stretch,  it is work.  I do not way.  it is impossible run on the debian Buster?

0 Kudos
Reply

1,601 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

You should ask to our third party since debian its not supported by nxp.

Regards

0 Kudos
Reply

1,601 Views
flyalfie
Contributor I

Hello Bio_TICFSL

        thanks  for your answer.   I try to downland debian-buster-sdhc img.  bug it can not boot from MMC

 U-Boot SPL 2018.11-08002-g8e521a3525 (Nov 20 2019 - 16:49:56 +0000)
PMIC: PFUZE100 ID=0x10
Training FAILED
Training FAILED
Training FAILED
Normal Boot
Trying to boot from MMC2
MMC Device 1 not found
spl: could not find mmc device 1. error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ##

0 Kudos
Reply

1,601 Views
flyalfie
Contributor I

I am try to boot loader for SD card. but it is no work

0 Kudos
Reply