MX8M-MINI RPA_v14

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MX8M-MINI RPA_v14

1,313 次查看
aviad_h
Contributor V

Hi,

Referring to the latest RPA " MX8M_Mini_DDR4_RPA_v14.xlsx" posted by NXP

According to revision table the CL setting (F28) for MT40A512M16LY-075:E has been updated to be in line with the datasheet and set to 17.

However in the datasheet of Micron P/N: MT40A512M16LY-075:E Table 1 for 075:E speed grade the CL value is 18 

Can you please explain the reason for the difference?

I wish to use Samsung P/N: K4A8G165WC-BCTD

it seems from datasheet Table 2 that CL=19 but this value is not an option in F28 drop down menu

Thank you for your support,

Aviad

0 项奖励
8 回复数

1,253 次查看
aviad_h
Contributor V

Hi,

Referring to Micron device, can you please explain your deduction of CL=17, is it according to speed grade -083 "READ CL: non-DBI"?

For that matter, why is that preferred over -083E, -083D corresponding values 16/18?

Thank you,

Aviad

0 项奖励

1,284 次查看
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   The Excel table (aid tool) comments parameter READ Latency (CL)
as following: "Please refer to the speed bin tables in the device
data sheet for CL settings that are supported for the chosen data
rate/clock cycle."

  The CL = 17 is taken from Table 158(DDR4-2400 Speed Bins and
Operating Conditions) of the memory Datasheet. Note: value CL=18
also is possible and may be considered as more "safe".

Regards,
Yuri.

0 项奖励

1,274 次查看
aviad_h
Contributor V

Hi,

The -075E ending of Micron P/N implies that speed grade is DDR4-2666 (See Table 1)

To my understanding "Table 159: DDR4-2666" is the corresponding table.1.png

Therefore my question is

1. Which is correct value for NXP Micron P/N: MT40A512M16LY-075:E

2. Which is correct value for Samsung P/N:  K4A8G165WC-BCTD ? Would 18 which is the max value in RPA tool be OK?

Thank you for your support,

Aviad

0 项奖励

1,263 次查看
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   1) It makes sense to use  timing parameters for the working memory frequency (DDR4-2400),
       but not for max  frequency (DDR4-2666).
  2) As for the Samsung device - please consult with them for assurance.

  

Regards,
Yuri.

0 项奖励

1,246 次查看
aviad_h
Contributor V

Hi,

Referring to Micron device, can you please explain your deduction of CL=17, is it according to speed grade -083 "READ CL: non-DBI"?

For that matter, why is that preferred over -083E, -083D corresponding values 16/18?

Thank you,

Aviad

0 项奖励

1,239 次查看
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   CL=17 configuration was tested.

Regards,
Yuri.

0 项奖励

1,234 次查看
aviad_h
Contributor V

Hi,

I apologize but the answer is not clear.

Can you please explain based on table 158 how this value was chosen, what cell in specific and why? if the value was selected arbitrarily and just tested please notify as well. This is required in order to be able to select correctly value for Samsung device.

Thank you for your support

Aviad

0 项奖励

1,232 次查看
Yuri
NXP Employee
NXP Employee

@aviad_h 

   You may select more "safe" value CL=18 (comparing with 17) and check it,
using the Stress memory test. If all is OK and there is - at least theoretical -
option CL=17 - why do not try and test it.
 

~Yuri.

0 项奖励