MX8-DSI-OLED1A color problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8-DSI-OLED1A color problem

Jump to solution
5,650 Views
nao_m
Contributor II

Hi,

I'm using an imx8M Plus with MX8-DSI-OLED1A panel. When I checked a ramp test pattern, some colors at low level have problem as the attached picture. It looks the blue bits are missing at low level.

I also checked HDMI output if this symptom occurs, but it didn't. This symptom occurs only on MX8-DSI-OLED1A.
Does anyone know how to fix this issue? Thanks.

Labels (1)
0 Kudos
1 Solution
4,880 Views
nao_m
Contributor II

Hello NXP TechSupport,

I purchased another display and confirmed this color issue was not occurred. It was a hardware issue.

Thank you so much for your support.

Thanks!

View solution in original post

17 Replies
5,631 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? Are you using the NXP i.MX8MP reference board?

0 Kudos
2,900 Views
YKL
Contributor I

我使用的硬件是i.MX8qm(MX8-DSI-OLED1A),下载的是官方的android_13.0.0_1.2.0演示图像。

显示的图像颜色不正确,无法触摸。

请帮帮我,谢谢!

 

0 Kudos
5,626 Views
nao_m
Contributor II

Hi,

BSP version is LF_v5.10.72-2.2.0, and yes, I'm using the i.MX8MP reference board.

Thanks!

0 Kudos
5,620 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the demo images? Or images you build yourself?

0 Kudos
5,612 Views
nao_m
Contributor II

It's a PNG image file. First, I found the color issue on my application demo. So, I tested with the PNG ramp pattern without the demo to make the issue simple. Stored the attached image in a directory and set "background-image" in weston.ini to the PNG file.

0 Kudos
5,588 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

How about running the demo images? Recommend you to use the demo images to have a test firstly, and share us the test result.

Wish you have a nice day

0 Kudos
5,575 Views
nao_m
Contributor II

Could you tell me where I can get the demo images and how to run them?

Thanks,

Tags (1)
0 Kudos
5,568 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The linux demo images links https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Android demo images linkshttps://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

You can follow the related user guide document to download and boot up board.

Then to see if the screen can display well or not.

0 Kudos
5,550 Views
nao_m
Contributor II

I might misunderstood the meaning of "demo". Actually, I'm using the Linux image that I downloaded from the link you shared. The color issue occurred on the Linux image. I didn't build the Linux image myself.
And I used uuu to update the Linux image on the board, executed uuu.auto that is stored in the LF_v5.10.72-2.2.0_images_IMX8MPEVK.

Thanks,

0 Kudos
5,518 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Does the system boot up success? And have you set the proper parameters for the OLED display, you can show us you u-boot command line and boot up log file to us? We can help check.

If it still not work, the screen maybe broken, you can apply to change new one.

0 Kudos
5,507 Views
nao_m
Contributor II

In u-boot, I set the following command to use MX8-DSI-OLED1A

U-Boot > setenv fdtfile imx8mp-evk-rm67199.dtb
U-Boot > run bootcmd

System looks working well after boot up. An application I created is running on the screen, and touch screen works.

Please find the attached bootup log.

Thanks,

0 Kudos
5,484 Views
nao_m
Contributor II

Hello, Have you found anything wrong in the boot-up log?
And, I was wondering if this issue is only in this particular display I'm using or could be reproduced in your side?

Thanks,

0 Kudos
5,463 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You boot up is OK, no problem. I have tested on our board for this screen, it works well. I run the demo images.

Can you give us your details steps?

0 Kudos
5,448 Views
nao_m
Contributor II

Thank you for taking your time to test on your board. The below is my details steps.

  • When I received a i.MX 8M Plus PEVK board, Linux Binary version "L5.4.70-2.3.2" was preinstalled in the board.
  • I downloaded the latest version of Linux image "LF_v5.10.72-2.2.0" from the NXP website, and I updated the Linux image on the board by uuu. I ran uuu.auto that is stored in the LF_v5.10.72-2.2.0_images_IMX8MPEVK. (I executed the command uuu -d uuu.auto from Windows PowerShell.)
  • Power on the board and edit /etc/xdg/weston.ini with adding the script below to remove menu-bar shown at the top of screen.

[shell]

panel-location=""

panel-position=none

  • Reboot the board and interrupt auto-boot in the serial terminal. Change the device tree file by entering the commands below.

U-Boot > setenv fdtfile imx8mp-evk-rm67199.dtb

U-Boot > run bootcmd

I ran an application I created, then I found this color issue, some level of gray color was green. To make sure if the issue is caused by my application or not, I displayed a ramp test pattern image without running my application as following steps.

  • Store ramp test pattern images under the root folder.(See attached files for testpatterns I used)
  • Edit weston.ini with adding the script below.

[shell]

background-image=/home/root/ramp_pattern.jpg

  • Reboot the board and change device tree to rm67199 in u-boot.
  • The color issue occurs in the ramp image.(See attached files for the color issue on display)

 

Thanks,

 

0 Kudos
5,416 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I am not sure it is caused by your application, another way is to run the Android BSP demo images in our website, to see if the screen can display or not, if it display still, this will confirm that it caused by the broken screen. You can try it and give me the feedback.

0 Kudos
4,881 Views
nao_m
Contributor II

Hello NXP TechSupport,

I purchased another display and confirmed this color issue was not occurred. It was a hardware issue.

Thank you so much for your support.

Thanks!

4,871 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it works well and thanks a lot for your kindly sharing.

0 Kudos