Hi,
I have recently purchased imx8mmevk board.
Now I've got L4.14.98_2.0.0_ga_image_MX8MMEVK in board,and there is a display on the 'MX8-DSI-OLED1'board.I did it according to the manual,but the error occured.the error followed:
u-boot=>setenv fdt_file fsl-imx8mq-evk-dcss-rm67191.dtb
u-boot=> run bootcmd
switch to partitions #0, OK
mmc1(part 0) is current device
** Unable to read file boot.scr **
23163392 bytes read in 283 ms (78.1 MiB/s)
Booting from mmc ...
** Unable to read file fsl-imx8mq-evk-dcss-rm67191.dtb **
WARN: Cannot load the DT
thanks.