MX7 with PF3000, Boost regulator and Supercaps

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX7 with PF3000, Boost regulator and Supercaps

ソリューションへジャンプ
985件の閲覧回数
demoniacmilk
Contributor IV

Our system uses an i.MX7D as its core, powered by a PF3000. Most of the systems peripherals are powered by an external 3V3 buck-boost regulator. Two supercaps in a row provide a <5V backup power source.

I am looking for a solution for the following scenario:
- All I/O Banks on the MX7 are connected to V33 (default @3.15V)
- All peripheral devices are connected to BUCKBOOST_3V3
- The buck-boost regulator is enabled by V33

- MX7 and peripherals are connected via I/O

- The systems main power fails and backup power is used

The Supercaps will discharge, resulting in a dropping backup voltage. While the voltage at the peripherals remains at 3V3 (Boost regulator), the voltage of V33 will begin to drop once the backup voltage has gone below 3V15+RegulatorDropout. As the maximum difference allowed between the I/O voltage on a connected pin and the internal I/O supply is 0.3 Volts, we get into a critical area once the input voltage drops too low, before the PF3000 finally turns off.

I am looking for a solution to keep the internal I/O voltages of the MX7 at 3V3 while the backup voltage drops.

The easiest solution is probably to connect all I/O bank supplies on the MC7 to the external Buck-Boost regulator, that is turned off once V33 is turned off. Would that be an exceptable solution or is there a constraint I am overlooking in this setup?

EDIT: the boost converter creates a small peak to 3V3 on startup, then drops back to about 1V before rising to 3V3 in a ramp

ラベル(2)
0 件の賞賛
返信
1 解決策
859件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lars

I believe such solution is also acceptable provided that power-up sequence

described in sect.4.1.9 Power-up sequence  i.MX 7Dual Family of Applications Processors Datasheet

will be satisfied.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
860件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lars

I believe such solution is also acceptable provided that power-up sequence

described in sect.4.1.9 Power-up sequence  i.MX 7Dual Family of Applications Processors Datasheet

will be satisfied.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------