MX7 USB - initialize but do not use USB Port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX7 USB - initialize but do not use USB Port

Jump to solution
1,591 Views
demoniacmilk
Contributor IV

Hello,

for a customer I have developed two different hardware versions of bascially the same product.

One difference between the two versions is the usage of the the USB OTG ports. One version uses both ports, the other uses just one.

So far, the USB OTG port that has not been used was not powered and had no external circuitry at all.

To allow my customer to use the same software on both versions (initializes borh ports) I would like to allow the unused USB port to be initialized in software. What is the minimal circuitry to allow this?

I guess: Power USB_OTGx_VDDA_3P3_in, attach a capacitor to OSB_OTGx_VBUS and a resistor to USB_OTGx_REXT? or may i cut some of these even?

thanks and regards,

Lars

Labels (2)
0 Kudos
Reply
1 Solution
1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

I believe you are correct, additionally capacitor at VDD_USB_OTGx_1P0_CAP

is needed for normal usb operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

I believe you are correct, additionally capacitor at VDD_USB_OTGx_1P0_CAP

is needed for normal usb operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply