Hello, I encountered a problem when debugging MX6Q. When burning the firmware with MfgTool2, it prompted No Device Connected.I have seen that debug is stuck in MMC. Could you please help me to see if there are any good Suggestions or relevant documents?Thank you very much.Here is the debug log
U-Boot 2018.03-00015-g6103ac6-dirty (May 22 2020 - 15:21:34 +0800)
CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 31C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
MMC:
解決済! 解決策の投稿を見る。
Hello,
I see that you're using imx_v2018.03_4.14.78_1.0.0 right?
If yes, please try with the latest MFGTool UUU, you may download it from here:
https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.154
uuu -> Linux version
uuu.exe -> Windows version
UUU.pdf -> Tool documentation
Regards,
Aldo.
Hello,
I see that you're using imx_v2018.03_4.14.78_1.0.0 right?
If yes, please try with the latest MFGTool UUU, you may download it from here:
https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.154
uuu -> Linux version
uuu.exe -> Windows version
UUU.pdf -> Tool documentation
Regards,
Aldo.
Thank you very much for your answer. My question has been settled