MX6Q stuck mmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6Q stuck mmc

Jump to solution
940 Views
icedustpan
Contributor II

Hello, I encountered a problem when debugging MX6Q. When burning the firmware with MfgTool2, it prompted No Device Connected.I have seen that debug is stuck in MMC. Could you please help me to see if there are any good Suggestions or relevant documents?Thank you very much.Here is the debug log


U-Boot 2018.03-00015-g6103ac6-dirty (May 22 2020 - 15:21:34 +0800)

CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 31C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
MMC:

Labels (2)
1 Solution
841 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you're using imx_v2018.03_4.14.78_1.0.0 right?

If yes, please try with the latest MFGTool UUU, you may download it from here:

https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.154

 

uuu -> Linux version

uuu.exe -> Windows version

UUU.pdf -> Tool documentation

 

Regards,

Aldo.

View solution in original post

0 Kudos
2 Replies
842 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you're using imx_v2018.03_4.14.78_1.0.0 right?

If yes, please try with the latest MFGTool UUU, you may download it from here:

https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.154

 

uuu -> Linux version

uuu.exe -> Windows version

UUU.pdf -> Tool documentation

 

Regards,

Aldo.

0 Kudos
841 Views
icedustpan
Contributor II

Thank you very much for your answer. My question has been settled