MX6 TOTALLY 4GBYTE RAM CONNECTION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX6 TOTALLY 4GBYTE RAM CONNECTION

545件の閲覧回数
dogancanyuksel_
Contributor I

I tried to find max ram capability and i found maximum memory which is 4gb dram memory.I try to 4gb totally DDR3 but i do not and i did not understand dram connection which is in added picture. It has 4gb dram memory but totally 2gb in these reference sheet. I do not understand. I need to help totally 4gb connection.

pastedImage_1.png

0 件の賞賛
1 返信

461件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

one can create service request for obtaining 4GB schematic example

How to submit a new question for NXP Support 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛