Hi,
In our application the IPU1 unit (at offset 0x2400000) should output 24 bit digital RGB through its DI1 to parallel port 1.
What we see is valid HSync and VSync signals (and RGB data signals) at parallel port 1, but no clock, nor a DE signal. Thus our externally connected TMDS encoder does not work.
We checked the physical connection by changing pad EIM_A16 to GPIO and it works as expected. But setting the MUX_MODE of pad EIM_A16 to ALT1 does not output any clock.
Are there any known restrictions connecting IPU1, DI1 to parallel port 1?
The used SoC pads are:
EIM A16 / ALT1 for display clock --> no signal at the pad
EIM D29 / ALT1 for display DE --> no signal at the pad
EIM DA11 / ALT1 for display HSYNC --> expected signal at the pad
EIM DA12 / ALT1 for display VSYNC --> expected signal at the pad
Solved! Go to Solution.
No, there are no known restrictions of operating the IPU1 DI1 parallel display port. The situation mostly looks like the software bug in configuring either IPU or IOMUX controller.
Have a great day,
Artur
No, there are no known restrictions of operating the IPU1 DI1 parallel display port. The situation mostly looks like the software bug in configuring either IPU or IOMUX controller.
Have a great day,
Artur
Hi Artur,
thanks for the feedback, in the meantime we found out about the reason. It was a pinmux problem that persisted over a (soft) reboot, so after we switched to powercycling the board after each attempt, the experiments were much more consistent, and in the meantime the board is running with two monitors attached.
Regards,
Robert