MX53 LVDS signal max length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX53 LVDS signal max length

Jump to solution
652 Views
ernstzberg
Contributor I

What is max length of MX53's LVDS signals ?

Labels (1)
0 Kudos
1 Solution
524 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ernst

I.MX53 LVDS interface complies with TIA/EIA 644-A standard.

Please refer to Table 7-6 "Application-Driven Decisions Used When Selecting Cable Media"

of the manual [known as former National_LVDS_Owners_Manual_4th_Edition_2008.pdf], linked below :

www.ti.com/lit/ml/snla187/snla187.pdf

Best regards

chip
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
525 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ernst

I.MX53 LVDS interface complies with TIA/EIA 644-A standard.

Please refer to Table 7-6 "Application-Driven Decisions Used When Selecting Cable Media"

of the manual [known as former National_LVDS_Owners_Manual_4th_Edition_2008.pdf], linked below :

www.ti.com/lit/ml/snla187/snla187.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos