MX51 mfw_vpuencoder works with yuv file, but not with videotestsrc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MX51 mfw_vpuencoder works with yuv file, but not with videotestsrc

跳至解决方案
2,745 次查看
RobbieJiang
Contributor IV

Hi,

I have been testing mfw_vpuencoder on MX51/Linux board.

Firstly, mfw_vpuencoder does not produce correct result with videotestsrc, but without any error message.

gst-launch-0.10 -v videotestsrc is-live=1 ! 'video/x-raw-yuv,format=(fourcc)I420,width=176,height=144,framerate=25/1'  ! mfw_vpuencoder codec-type=std_avc width=176 height=144 framerate=25 !  filesink location=test_1.264

The generated output file (test_1.264) is quite different from the input test video.

However, if I firstly generate a test.yuv using videotestsrc, and encode the test.yuv with mfw_vpuencoder, it works well.

gst-launch-0.10 -v videotestsrc is-live=1 ! 'video/x-raw-yuv,format=(fourcc)I420,width=176,height=144,framerate=25/1'  ! filesink location=test.yuv

gst-launch -v filesrc location=./test.yuv ! mfw_vpuencoder codec_type=std_avc width=176 height=144 gopsize=10 framerate=25 ! filesink location=test.264

This time, the output file (test.264) is almost the same as the input file, test.yuv, which means that mfw_vpuencoder works well as desired.

Anything wrong with my videotestsrc + mfw_vpuencoder encoding pipeline?

FYI, my kernel is 2.6.31, imx-lib-10.04, gst-fsl-plugin-1.7.3.

And the imx-test/mxc_vpu_test.out works correctly with config_enc file.

Regards,

Robbie

标签 (3)
1 解答
2,243 次查看
LeonardoSandova
Specialist I

Try this pipeline

gst-launch-0.10 -v videotestsrc is-live=1 blocksize=38016 ! \

     'video/x-raw-yuv,format=(fourcc)I420,width=176,height=144,framerate=25/1'  ! \

     mfw_vpuencoder codec-type=2 width=176 height=144 framerate=25 !  \

     filesink location=test_1.264

where blocksize= width * height * 1.5. Also, please try with other codecs. In case the camera is working, you can also try a real live source with the following pipeline

gst-launch mfw_v4lsrc fps-n=15 capture-width=$WIDTH capture-height=$HEIGHT ! \

     queue ! \

     mfw_vpuencoder codec-type=0 ! \

     avimux ! \

     filesink location=output.avi sync=false

In case you dont have the documentation, please refer to https://www.freescale.com/webapp/Download?colCode=IMX51_1011_MMDOCS_BUNDLE&location=null&fpsp=1&WT_T...

Leo

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,243 次查看
FranciscoCarril
Contributor V

videoTestSrcimx51.JPG

This test was run with i.MX51,   with your first pipeline, so  you are using the correct pipeline,   you might be missing some plugin or patch.

You can download the linux patches here:

https://www.freescale.com/webapp/Download?colCode=IMX_ER_1011_LINUX_PATCHES&appType=license&location...

BSP 10.11.01

kernel 2.6.35

10.11.01 patches from web page applied.

MM codecs 10.11  ->  fsl plugin and gst plugin  1.9.5

Selected Gstreamer "Good"  package.

0 项奖励
回复
2,243 次查看
RobbieJiang
Contributor IV

Hi Francisco,

Thank you.

I finally passed the test by setting the "peer_alloc" property of videotestsrc to false.

2,243 次查看
FranciscoCarril
Contributor V

What is the effect you are seeing?

With your first pipeline I had to remove the framerate from the mfw_vpuenc , since it caused error, but after that, it generated this video.

and this is my resultvideotestphoto.JPG

0 项奖励
回复
2,243 次查看
RobbieJiang
Contributor IV

Here is my result:

Screenshot-test-err.264-1.png

And what's your kernel version, imx-lib version and gst-fsl-plugins version?

0 项奖励
回复
2,244 次查看
LeonardoSandova
Specialist I

Try this pipeline

gst-launch-0.10 -v videotestsrc is-live=1 blocksize=38016 ! \

     'video/x-raw-yuv,format=(fourcc)I420,width=176,height=144,framerate=25/1'  ! \

     mfw_vpuencoder codec-type=2 width=176 height=144 framerate=25 !  \

     filesink location=test_1.264

where blocksize= width * height * 1.5. Also, please try with other codecs. In case the camera is working, you can also try a real live source with the following pipeline

gst-launch mfw_v4lsrc fps-n=15 capture-width=$WIDTH capture-height=$HEIGHT ! \

     queue ! \

     mfw_vpuencoder codec-type=0 ! \

     avimux ! \

     filesink location=output.avi sync=false

In case you dont have the documentation, please refer to https://www.freescale.com/webapp/Download?colCode=IMX51_1011_MMDOCS_BUNDLE&location=null&fpsp=1&WT_T...

Leo

0 项奖励
回复
2,243 次查看
RobbieJiang
Contributor IV

Hi Leo,

Finally I managed to do this with the following pipeline:

gst-launch-0.10 -v videotestsrc is-live=1 peer_alloc=false   ! \

     'video/x-raw-yuv,format=(fourcc)I420,width=176,height=144,framerate=25/1'  ! \

     mfw_vpuencoder codec-type=2 width=176 height=144 framerate=25 !  \

     filesink location=test_1.264


Note that "peer_alloc" must be sest to "false".  I don't know why, but it did work for me.

And this is very different from what I have done on MX27 (on MX27, no need to change peer_alloc. the default value is OK.), and also quite different from your pipeline.

gst-inspect videotestsrc:


  peer-alloc     

: Ask the peer to allocate an output buffer
                    flags: readable, writable
                    Boolean. Default: true Current: true

The default value of peer_alloc is true, which requires mfw_vpuencoder  allocate an output buffer. 

Perhaps something is different for MX27 VPU and MX51 VPU?

I have been also able to get mfw_vpuencoder work with ov7725 camera without any problem.

Thank you.

0 项奖励
回复